Beta Features In Use
The Beta Features In Use indicator displays the number of Beta features in use in the current measurement(s). This indicator is displayed on the status bar just to the left of the Reference status indicator. It appears only when at least one feature is being used that is in a Beta (pre-release) state.
Beta features may not be fully developed, tested or documented, and they are not supported as part of the released product.
Right-click this area to open a dialog that lists all currently used Beta feature(s) and provides details about each feature.
See Also